Web Reports Issues

If the Plant Applications Web Reports are not working correctly, you may need to enable HTTP Keep-Alives.

About this task

For information about installing and using SSRS, refer to the Proficy Plant Applications SSRS Report Configuration and Report Creation Guide, which is posted in KB16011.

Procedure

  1. In the Internet Information Services (IIS) Manager, locate the local computer.
  2. Expand Web Sites, right-click the website, and then select Properties. The Properties dialog box for the web site is displayed.
  3. On the Web Site tab, click Connections and ensure Enable HTTP Keep-Alives is selected.
  4. Click OK.