Plant Applications Server and Client Requirements
Before you install Plant Applications, verify that all required software versions have been installed on the target machine.
Workflow is required for Plant Applications and can be installed from the Installation Menu.
See Test and Production Environments to compare machine requirements in a test, standard production, and high-transaction environment.
Operating System
- Microsoft® Windows® Server 2019 (64-bit) for server installations
- Microsoft® Windows® Server 2016 (64-bit) for server installations
- Microsoft® Windows® Server 2012 R2 (64-bit)
- Microsoft® Windows® 10 (64-bit) for Client installations
Network Interface Software
- Internet Protocol Version 4 (IPv4)
Microsoft®.NET Framework
- Microsoft .NET Framework 4.7 for Workflow 2.6 SP1Note: You can download the Microsoft .NET Framework 4.7 from the following URL: https://go.microsoft.com/fwlink/?LinkId=825299
- Microsoft .NET Framework 4.7.2 for Plant Applications Server
- Microsoft .NET Framework 3.5 for Plant Applications Client
Microsoft® SQL Server®
- Microsoft® SQL Server® 2019 (with mandate Cumulative Update 4 installed), 2017 (64-bit), and 2016 (64-bit)Note: You must have SQL Server 2016 (64-bit) or later for the Plant Applications Server and Web Client installation. If you are running a previous version of SQL Server, a message stating that the prerequisite criteria not met appears. You must upgrade to SQL Server 2016 (64-bit) or later to continue with the installation.
- Microsoft System CLR Types SQL Server 2016 (32-bit only)Note: Do not install if you already have the Microsoft System CLR Types SQL Server 2016 (32-bit only) installed.
- SQL Server 2012 Native Client version 11.4.7001.0 or laterNote: The SQL Server 2012 Native Client is required for Plant Applications Server and Plant Applications Client machines. If the version of the SQL Server 2012 Native Client you installed is not 11.4.7001.0 or later, you must upgrade it. You can download the SQL Server 2012 Native Client version 11.4.7001.0 or later from the following URL: https://www.microsoft.com/en-us/download/details.aspx?id=50402
- For information on SQL Server requirements, refer to SQL Server Requirements.
Software Requirements
Software | Requirement |
---|---|
Web Server | IIS 8.0 or later based on the operating system |
Microsoft Office | Microsoft Excel 2019, 2016, or 2013 (required for SQL Server and Web Engines) 32-bit. Note: If you import data using a Microsoft Excel file that was created in an older version, it will not contain the columns necessary to support the new Event Progress feature. Refer to topics in Plant Applications Help for steps describing how to use the Excel add-in. |
Document Viewer | PDF reader (required to view some Web Server reports) |
Workflow | Workflow 2.6 SP1 Note: You must install Workflow 2.6 SP1 if you are installing a clean environment of Plant Applications.
|
Browsers |
Note: Process Analyzer only supports Chrome.
|
Communication | MAPI-compliant Mail client software |
Server Hardware Requirements
Minimum Requirement | GE Recommended |
---|---|
The minimum server requirements when running a Plant Applications environment without SOA entities and not using the Client or Workflow:
|
For a standard implementation, GE recommends the following:
|
Client Hardware Requirements
- Pentium 4-based computer with 2 GB of RAM (minimum)
- 20-GB hard drive space (minimum)
- DVD drive
- Network interface software for network communications supporting TCP/IP
- Monitor for the lab and floor operations, 100 percent IBM compatible, supporting a 24-bit graphics card for 1024 x 768 or higher resolution and at least 65535 colors
- Two-button mouse with scroll wheel or compatible pointing device such as a touch screen
Supported Small Screen Devices
- iPad 6th Gen: Safari v13.1+, Chrome 85.0 or later with resolution 2048x1536
- HP tablet: Chrome 85.0 or later , with minimum resolution 1920x1280
- Activities
- Downtime
- OEE Dashboard
- Reports
- My Machines
- Alarms
- Process Orders
- Waste
- Operator
- Work Queue
- NCM
Port Requirements
Port | Description |
---|---|
80 | Used by Web server for serving traditional, web reports. |
15672 | The default port for the RabbitMQ Message bridge required to communicate with the Plant Applications server for retrieving data updates. |
Use the CXS_Service
table in the Plant Applications database to modify the following ports:
Port | Description |
---|---|
12293 | Used by Proficy Server Manager for the Service Control feature of the Administrator. |
12294 | Used by Proficy Server Gateway for clients (including SDK) to send/receive Plant Application messages. |
12295 | Used by Proficy Server Gateway for clients (including SDK) to send/receive Plant Application messages. |
12295 | Used by older (4.0 and older) versions of Client Manager. |
12299 | Used by Proficy Server Remote Data Service, allowing Proficy services perform remote read and write operations to a historian. |
12401 | Used by Proficy License Manager for licensing requests from Proficy services to clients. |
5762 | Used internally by Plant Applications services to connect to RabbitMQ. |
Use INI files such as cmRTR.ini, cmConfigMgr.ini, PlantAppsMessging.ini, or Message.ini(found in the Plant Applications program installation directories), to modify the following ports.
Port | Description |
---|---|
10000 | Used by the Proficy message router to process Plant Applications messages between services clients communicating with the router. |
12280 | Used by the Proficy message router to process Plant Applications messages between services clients communicating with the router. |
Use internal interfaces to open the ports required for Operations Hub.
Port | Description |
---|---|
443 | Used by Operations Hub |
Use internal interfaces to open the ports required for an SQL server.
Port | Description |
---|---|
1433 | Used by SQL Server |
Use internal interfaces to open the ports required for a Couch server.
Port | Description |
---|---|
6984 | Used by CouchDB Server |
Use internal interfaces to open the ports required for the Plant Applications Web Client node.
Port | Description |
---|---|
5059 | Used by the Plant Applications Web Client node |
9093 | Used by the Plant Applications Web Client node |
Languages Supported for Translation
Languages | Plant Applications Client | Plant Applications Web Client 8.x | |
---|---|---|---|
Process Available in versions above |
Discrete Available in versions above |
||
US English | YES | 8.0 | 8.0 |
Arabic | YES | 8.0 | 8.1 |
Bosnian | YES | 8.2 | |
Chinese (Simplified) | YES | 8.0 | 8.1 |
Czech | YES | 8.1 | 8.1 |
Danish | YES | 8.0 | |
Dutch | YES | 8.0 | |
Finnish | YES | 8.0 | |
French (European) | YES | 8.0 | |
German | YES | 8.0 | 8.2 |
Hebrew | YES | 8.0 | |
Italian | YES | 8.0 | |
Japanese | YES | 8.0 | 8.1 |
Korean | YES | 8.0 | |
Russian | YES | 8.0 | 8.2 |
Polish | YES | 8.0 | |
Portuguese (Brazilian) | YES | 8.0 | |
Slovenian | YES | 8.0 | |
Spanish (Latin American) | YES | 8.0 | 8.2 |
Swedish | YES | 8.0 | |
Turkish | YES | 8.0 | 8.2 |
Vietnamese | YES | 8.1 | 8.1 |
Compatibility with Other GE Products
GE Software | Supported Version |
---|---|
Operations Hub | 2.0, 2.1, or 2022.06 |
Workflow | 2.6 SP1 |
Historian | 8.1, 9.0 and 9.1 |
iFix | 6.1 and 6.5 |
CIMPLICITY | 11.0 and 11.1 |