Uninstall Plant Applications

About this task

This procedure is applicable if you want to uninstall the Plant Applications and its components from your system.

Procedure

  1. From the Windows Start menu, select Control Panel > Programs > Programs and Features.
  2. From the list of applications, uninstall programs in the following order.
    1. Proficy Plant Applications Client
    2. Proficy Plant Applications Web Server
      Note: When uninstalling Web Server, ensure that you close all the Plant Applications windows or instances. You may encounter an Failed to unregister PRUtils.dll error message during uninstallation. You can ignore this message and select OK.
    3. Proficy Plant Applications Server
  3. Optional: If you have installed Service Packs or SIMs for Plant Applications, from REGISTRY (regedit.exe), you must manually remove SIM entries from the registry key: HKEY_LOCAL_MACHINE\Software\Wow6432Node\Microsoft\Windows\CurrentVersion\Uninstall.