Verifying the Server Connection
When using Plant Applications, the connection to the server can be lost for a number of reasons.
Procedure
- Start Plant Applications Administrator and log in with username comxclient and password comx.
- Start Plant Applications client and log in with username comxclient and password comx.
- Start Microsoft Excel.
- Load the Plant Applications Add-in for Excel, click .
- Connect to the Plant Applications Server. For more information, see Connecting to a Server topic in the online help for the Add-in.