The Add User Defined Event window appears, displaying a list of user-defined autolog sheets accessible to you as configured in Plant Applications Administrator.
In the Choose activity section, select an activity to create a user-defined event on the selected activity.
In the Add Event Details section, in the EVENT NUMBER box, enter a unique event number.
In the DURATION box, select a start and end time for the event.
Optional: Specify values for the following properties: STATUS, APPLIED PRODUCT, and COMMENT.
Note: When the status of a user-defined event associated with the activity is set to a production status that has the Lock Event Data option enabled, you do not have the privilege to modify the autolog sheet for that event.
In the REASONS box, select a reason to create a user-defined event.
Select Save.
Results
The user-defined event for the selected activity is added and an activity is automatically created for the event. The activity appears in the Open page.