As an operator or a supervisor, you can access the following types of activities:
You can also:
By default, the option to automatically refresh activities is disabled. You can switch
the toggle to enable or disable the option to automatically refresh the page as
described in the following table. After you select an option, your selection is
saved.
Option |
Description |
 |
When this option is selected:
- If
appears in the
Open page, additional completed or
skipped activities are available in the shift. Select to refresh the page and
access all the completed or skipped activities.
- If
appears in the
Completed page, no additional
completed or skipped activities are available to access.
- If
appears in
the Completed page, the RabbitMQ
service is down.
|
 |
When this option is selected:
- If
appears in the
Completed page, the manual refresh
option is disabled. The page automatically refreshes when an
additional completed or skipped activity is available.
- If
appears in
the Completed page, the RabbitMQ
service is down.
|
The number of records displayed in the page depends on the value that is
configured for the
maxRecordsToFetch property in the
app.properties.json file. The location of this file depends on
the type of installation:
- Enterprise installation: <Install
Directory>/PlantApplicationsDocker/plantapps-web-docker/mnt/configfiles/activities-app/prod/{{appVersion}}/<appname>.yml
- Standard installation: <Install
Directory>\config-rep\activities-app\prod\{{appVersion}}\<appname>.yml
If the number of records in the database is more than the value configured for the
maxRecordsToFetch property, a notification to contact the
administrator appears.