About Process Orders
- All Units Run Same Schedule Simultaneously: This setting is used in production process that are running very fast and producing product at a high rate. This allows multiple Production Units to run against the same Schedule at the same time.
- Schedule Flows By Event: This setting allows a Process Order to flow through the process with the Production Event. When the Production Event is loaded on to the next Production Unit, the Process Order will follow that Event and become the Active order on that next Unit.
- Schedule Flows Independently: In this setting, Process Orders need to be pushed to the next Production Unit. The Order can be pushed manually or automatically. The Operator can push the Process Order from one Production Unit to the next. The Order can be pushed automatically through models. This can be done with various triggers that can be watched by a model.
As a supervisor, you can use the Process Orders application to perform the following actions:
- Access Open Orders
- Access Closed Orders
- Access Details of a Process Order
- Add a New Process Order
- Modify a Process Order
- Delete a Process Order
- Advance a Process Order
- Add Comments to a Process Order
- Modify Process Order Comments
- Delete Process Order Comments
- Modify a Process Order Status
- Sequence a Process Order