Modify a Process Order

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select .
    By default, the Open page appears, displaying a list of process orders grouped based on the multiple execution paths (configured in Plant Applications Administrator) or unbound path in a tabular format.
    Note: If the Display Unbound Process Orders display option is set to True (this value is set in the Display Options from the Plant Applications Administrator), the unbound Process Orders are displayed below the Unbound category, with no Path column displayed.
    You can select the Closed tab if you want to edit process orders that are in the completed status.
  3. From the Actions column, select for a required process order.
  4. From the menu, select Edit.
    The Edit Process Order page appears.
  5. As needed, modify process order parameters as required in the General and Advanced sections.
    Note: When you associate a bill of materials formulation with a process order, only the formulations associated with the selected product will be available for selection.
  6. Optional: If the selected process order is not bound to a path, in the General section, you can use the PATH field to bind the process order to a path.
  7. Optional: In the General section, select Add Comments to either add, modify, or delete comments for the process order.
    The Add Comment window appears.
  8. In the ADD COMMENT box, enter a comment for the changes you made, and select Add.
    Note: You can modify or delete only those comments that were added by you. However, based on the site parameter, you can also update comments from other users if you have the required permissions.
  9. Select Save.
    Note: The changes made to the process order are saved.