By default, the Open page appears, displaying a list of process orders. You can select the Closed tab if you want to change the status of process orders that are in the completed status.
From the Actions column, select for a required process order.
Based on the current status of the process order, you can perform any of the following actions:
If the current Status is Pending, then you can either select Next or Planning based on the valid transition states configured for the execution path to which the process order belong.
If the current Status Next, then you can select Active or Pending based on the valid transition states configured for the execution path to which the process order belong.
Note: Activating a process order makes it the current running process order that product quantities, process order run times, and process order statistics are applied to.
If the current Status Active, then you can select Complete or Pending based on the valid transition states configured for the execution path to which the process order belong.
Note: For a given execution path, you can have only one process order that is in active or next state. Completing an Active process order allows a different process order to be activated. If another process order has a status of Next, it will automatically become the Active process order when the current Active process order is moved to Complete.
Optional: Alternatively, you can change the status of a process order from the Process Order Details page.
In the Process Order Details page, select and then select the required status from the available options.