Sequence a Process Order

About this task

By default, process orders are sorted by schedule status, then implied sequence (descending), and then forecast start date. In the Open page, a selected process order that is in pending status can be moved up or down one row on the path it is bound to (switching places with the process order above or below it).

Procedure

  1. Log in to Plant Applications Web Client.
  2. Select .
    By default, the Open page appears, displaying a list of process orders grouped by the associated execution path in a tabular format.
  3. From the Actions column, select or for a required process order that is in the pending status to move up or down one row on the path it is bound to.