Variables are measurements or calculations attached to a given production unit that
produce values either by time or event. Variables are created in
Plant Applications Administrator. Using the
Activities
application, you can:
The following conditions apply when you enter or modify a variable value:
- You must configure a variable and include that variable on an autolog display
using Plant Applications Administrator.
- You must create an activity
for the autolog variable.
- If the data source of the variable is Historian or Calculation Manager, you must have the Admin privilege. Note that when the
data source is Historian or Calculation Manager, the variable already contains a value, and you can
only modify the value.
- If the data source of the variable is Autolog, you must have the Read/Write,
Manager, or the Admin privilege.
- In Plant Applications Administrator, when the status of a production-based or user-defined event associated with
the activity is set to a production status that has the Lock Event
Data option enabled, you do not have the privilege to modify the
autolog variables.
- In Plant Applications Administrator, if the LockUnavailableCells option is enabled for the
display associated with the activity, only the users in the Administrator
security group with an access Level other than Read can enter values for the
modifiable autolog variables that have no available data.