To complete an activity, you must perform the following tasks:
- Enter values for all the mandatory variables in the activity.
- If it is mandatory to enter a comment for an overdue activity, enter the comment.
- Mark the activity complete.
The following conditions apply when you complete an activity:
- If there are mandatory variables for the activity, you must enter values for all of them (that is, the status of the activity must be 100%).
- If the Overdue Task Requires Comment option is set to true in the sheet display options in Plant Applications Administrator, and if the activity is overdue, you must add an overdue comment.
- If the option to lock activities is set to True in Plant Applications Administrator, when you select Perform for an activity, the activity is locked and the In Progress option appears for the activity. Another operator cannot perform the activity until you release the activity.
- If the System Complete Activity On New Event option in Plant Applications Administrator is enabled for the display, and you create an activity inPlant Applications Web Client whose product ID, process order ID, and unit ID match those of any existing activities, the existing activities are automatically set to complete. Depending on the number of such existing activities, the application might take some time to set all the activities to complete. You can then perform only the new activity that was last created.