Access the Autolog History of a Completed Activity

About this task

The autolog history contains the overall details of the event associated with an activity and a maximum of 20 historical values of autolog variables entered for the event at different durations when the activity was scheduled.

You can access the autolog history of only a completed activity.

Procedure

  1. Access the activity whose autolog history you want to access.
    The autolog history of the activity appears. The following table describes each column.
    Column Description
    Event Name The unique ID of the event.
    Date The current date and time in the format dd/mm/yyyy hh:mm:ss (for example, 27/03/2022 10:58:29).
    Process Order The process order associated with the event.
    Product The product associated with the process order.
    You can select any of the three views based on the specifications:
    • Data: Displays only the autolog variable details.
    • Spec: Displays only the autolog variable box, which is colored based on the specification limits for the autolog variable as configured in Plant Applications Administrator.
    • Data & Spec: Displays the autolog variable details along with the background color based on the specification limits.
  2. If you want to view the specification limits and the colors associated with them, select View Legend.
    The following specification limits appear:
    • Reject
    • Warning
    • Target
    • User
    • Unavailable
  3. Select an autolog variable.
    If the specification limits for an autolog variable are available, the following information appears:
    • The lower and upper specification limits
    • The specification limit associated with the variable based on the value entered for the variable
    • The threshold value based on whether the entered value is higher or lower than the target value