Add a Production-Based Event

Procedure

  1. Log in to Plant Applications Web Client.
  2. In the application navigation menu, select .
    The Open page appears.
  3. Select , and then select Production Based Event.
    The Add Production Event window appears, displaying a list of production-based Autolog sheets accessible to you as configured in Plant Applications Administrator.
  4. In the Choose activity section, select an activity that you want to create for the event.
  5. In the Event Details section, in the EVENT NUMBER box, enter an event number that is unique per unit.
    Note: If the string of the event number of the last added event has numeric values in it, the application automatically increments the last numeric value by 1. The string with the incremented numeric value for the new event appears in the EVENT NUMBER box. You can retain or modify this value. For example, if the event number of the last added event is PB79RQ89AP, the value PB079RQ90AP appears in the EVENT NUMBER box for the new event. Similarly, if the event number of the last added event is PB79RQ89AP1, the value PB79RQ89AP2 appears in the EVENT NUMBER box for the new event.
  6. In the DURATION box, select a start time and end time for the event.
    The start and end time of the event must be within two hours from the current date and time.
  7. Optional: Enter values for the following properties: STATUS, APPLIED PRODUCT, and COMMENT.
    Note: When the status of a production-based event associated with the activity is set to a production status that has the Lock Event Data option enabled, you do not have the privilege to modify the autolog variables for that event.
  8. Select Save.

Results

The production-based event for the selected activity is added, and an activity is automatically created for the event. The activity appears in the Open page.