Returning a Lot
Before you begin
- To return a lot that was consumed, you must have the Return raw material permission. If you do not have the permission to perform this task, request your administrator to provide the permission using Security application. For more information, refer to Create a Role.
- To return a lot that was consumed, you must clock on the operation of the lot. If the operation is not clocked on, the Return button is not enabled. Refer to Clock on Serials/Lots for an Operation to clock an operation.
About this task
Procedure
- Log in to Plant Applications Web Client.
- Select Work Queue.
-
Select the operation whose BOM items you want to access.
The BOM section appears, displaying the BOM items associated with the selected operation.
-
Select the BOM item that you want to return.
A window appears, providing information on the required quantity of the BOM item, and the quantity that has been already consumed for the serial/lot. By default, the Consumption History section is displayed in the Consume tab, and when you select the Return tab the Consumed Lots section is displayed.
-
Select the Return tab.
The Consumed Lots section is displayed.
The following table provides information on each column in the Consumed Lots section.
Column Description SERIAL/LOT# The serial/lot of the raw material. CONSUMED QTY The actual quantity of the serial/lot consumed while executing an operation. AVAILABLE QTY The quantity available for consumption. The quantity available is updated accordingly if the consumed quantity is returned. STATUS The status of the serial/lot. UOM The unit of measure (UOM) of the BOM item. MATERIAL The material number of the serial/lot. -
Enter the serial/lot number that you want to return in the SCAN
SERIAL/LOT# field.
Tip: Click the serial/lot number that you want to return in the SERIAL/LOT# column from the Consumed Lots section. The selected serial/lot number will be displayed in the SCAN SERIAL/LOT# field.
-
Enter the quantity that you want to return in the QUANTITY
field.
Note:
- You can only return the serial/lot that is consumed.
- You can not return more than the consumed quantity.
-
Select one of the valid statuses in the STATUS drop-down
box. You must select the status as configured in Plant Applications Administrator for that serial/lot.
Note:
- The required status is configured on the unit where the serial/lot is created.
- If you are a Plant Applications Administrator, you can do any of the following:
- Add the required status to the valid status list, using Unit Properties Configuration in Plant Applications Administrator > Plant Model.
- Configure the status of the serial/lot to one of the valid statuses using Production Status Editor in Plant Applications Administrator > Global Configuration.
-
Select the NCM Enabled checkbox.
The Create Non Conformance window appears.
-
Enter details for the following, then select Submit.
- SUMMARY
- DEFECT TYPE
- DEFECT REASON
A non-conformance is created for the serial or the defective pieces of the lot, and appears in Non Conformance. -
Select the Return button.
The Consumed Lots section is updated. The value of CONSUMED QTY and the AVAILABLE QTY is updated accordingly.