Provide Data for Quality Variables
About this task
Quality variables include details about the data that you must collect while performing an operation. These variables are defined in Plant Applications Administrator. The values that you provide for these variables help verify that the parameters that are critical to the quality and manufacturing processes are within the acceptable limits. You can use this data to review the performance of a production line and production unit and compare the quality of the products produced in each unit with projections for an operation.
For example, suppose you have been assigned the testing operation in a motor manufacturing unit. Quality variables can include the torque and rpm of the motor shaft. When you test each motor, you must enter the torque and rpm values for the corresponding serial number. A quality supervisor can then verify that the torque and rpm fall within the acceptable range.
For an operation that requires clocking on, you can mark the operation complete only after you provide data for all the mandatory quality variables. For an operation that does not require clocking on, however, you can mark the operation complete even if you have not provided data for the mandatory quality variables.
Before you begin
Procedure
- Select the operation for which you want to provide data for the quality variables.
- Select Quality.A list of serials/lots in the operation appear in the left section.
- Select the serial/lot whose data you want to provide.A list of quality variables defined for the operation appear in the workspace.Tip:
- By default, all the quality variables appear. If you want to access only mandatory variables, select Mandatory Variables in the drop-down list box.
- To add a Manual Historian Variable, see Add a Manual Historian Variable.
- If you want to view the lowest, highest, lower quartile, upper quartile, and median values for each variable, select
. If you want to view the same values plotted on a chart, select
.
- For each variable, enter data in the SPEC column. Tip: If you want to plot the value on a chart, select
.
If acceptable limits have been specified for the variable, the box in the SPEC column displays a color, indicating whether the value that you have entered is within the acceptable range.Note: If the variable has electronic signature enabled, an Electronic Signature window appears whenever you insert or edit a test value for a variable. Theicon near the text box indicates that the variable is entitled to electronic signature for any modifications. For more information about electronic signature, refer Modify the Value of an Electronic Signature Autolog Variable.
- Repeat steps 3 and 4 for each serial/lot in the operation.
Results
What to do next
"No serial lots are eligible to complete as mandatory BOM (or) Quality are pending (or) at least one variable is out of specification."
Furthermore, the non-conformance/defect will need to be disposed from the Non Conformance application. Once a defect has been created, the quality variable that was out of specification will become disabled and you cannot modify or update the value.