Submit Inspection Results
Before you begin
Procedure
- Select Inspection Results.A list of serials/lots in the material lot appears.
-
You can update the status of serial/ lot in the following methods:
- If you want to update the status of a specific serial/lot, for that serial/lot, in the STATUS column, select an option as needed.
- If you want to update the status for multiple serials/lots
simultaneously, select the check boxes that are available beside the
required serials/ lots or to select all the serials/ lots, select the check
box that is available on the table header row. Once you select the required
serials/ lots, select the suitable status from the status drop-down box that
is available beside the search box.Note:
- For multiple selection of serials/ lots, you can change the
status only in the following sequence:
- Open to MRB/NCR or Accept
- MRB/NCR to Open
- You can only accept the serials/ lots that have all conforming tests.
- You can mark the serials/ lots that are not inspected (quality variables are not filled) as MRB/NCR directly.
- For multiple selection of serials/ lots, you can change the
status only in the following sequence:
Option Description Accept Select this option if you want to accept the inspection results for the serial/lot. MRB/NCR Select this option if the serial/lot is defective and you want to create a non-conformance. It is then available for the material review board (MRB) to dispose the defect. The status of the receiver is then indicated by .
Open The options that you have selected for each serial/lot are saved. - If you have accepted all the serials/lots in the material lot, select Submit. If, however, you want to create a non-conformance for at least one of them:The inspection is complete (indicated by
). The inspection now appears in the Closed section. You can no longer modify the inspection results.