STATUS |
The status of the defect. |
SERIAL/LOT# |
The serial/lot number of the defective part. You can
select the link in this column to search for all the defects
associated with the serial/lot. |
PLAN |
The disposition plan created for the defect. You can
select the link in this column to search for defects
associated with the disposition plan. For a defect in the
Submitted state, the value in this column is blank. |
OP |
The operation during which the defect was
created. |
MATERIAL |
The material of the defective part. You can select the
link in this column to search for defects associated with
the material. |
MATERIAL FAMILY |
The material family associated with the defective
serial/lot. |
AFFECTED QUANTITY |
The quantity of the defective serials/lots for the
non-conformance. For a serialized product, the value in this
column is always 1. |
MATERIAL DESC |
The description of the material of the defective
serial/lot. |
RECEIVER NUMBER |
The name of the receiver material lot. This field is
populated when a defect is created on material lot(s) in the
Receiving Inspection app. |
DISP |
The method of disposition performed on the defective
serial/lot. For a defect in the Submitted status, the value
in this column is blank. |
CTP/REWORK OP |
The operation until which a defective serial/lot can be
processed before disposing the defect. This is applicable
only if the disposition method for the defect is
Continue-to-Process (CTP). During the operation specified in
this column, the defect must be disposed. |
NC |
The unique identifier automatically generated by the
application when the non-conformance was created. |
WORK ORDER |
The name of the discrete work order. |
DEFECT REASON <number> |
The hierarchy of reasons identified for the
defect. |
UNIT |
The name of the equipment or unit. For defects created in
discrete apps, the unit is associated with the operation the
defect is created on. For defects created in Receiving
Inspection, the unit is associated with the material lot it
is based on. |
ACTION REASON <number> |
The hierarchy of actions identified for the
defect. |
DEFECT MODIFIED BY |
The last user who modified the defect. |
DEFECT MODIFIED ON |
The date and time the defect was last modified. |
DEFECT ID |
The unique identifier automatically generated by the
application when the non-conformance was created. |
SUMMARY |
The brief description of the defect/non-conformance that
was entered when the non-conformance was created. |
ACTIONS |
The actions you can perform on the serial/lot. Contains
the following buttons:
: Select this button
to dispose the defect. This button is enabled
only for a defect in the Submitted status.
: Select this button to
modify the non-conformance details. This
button is enabled only for a defect in the Submitted
status.
: Select this button, and
then select Remove from Plan
to remove the defect from a disposition plan.
|