Add Defects to a Disposition Plan
About this task
If the disposition method and reasons for multiple defects are the same, you can dispose them at the same time. To do so:
- Add the defects to a new or existing disposition plan.
- Dispose the defects.
You cannot add a defect to a plan if:
- The defect is created for a non-serialized product.
- The defect is already added to a plan.
Procedure
- Access a non-conformance by performing one of the following tasks:
- If the non-conformance appears in the workspace or in the left pane, select the link.
- Enter the non-conformance number in the Search box that appears in the left pane or in the workspace.
All the defects associated with the non-conformance appear in the workspace. - Select the check box corresponding to each defect that you want to add to a plan.Note: The check box appears only if the defect is for a serialized product and if the defect is not added to a plan.Tip: To select all the defects for a non-conformance, select the check box in the heading column.
- Select
.
The Create a Plan or add to an existing Plan window appears, displaying a list of plans. - If you want to add the defects to an existing plan, select the plan, and then select Apply.The selected defects are added to the plan.Tip: You can search for an existing plan using the Search box.
- If you want to add the defects to a new plan, select Add to a New Plan, and then select Apply. A plan is created with a system-generated name, and the selected defects are added to the plan.
- Repeat steps 1 through 5 to add defects from other non-conformances to the plan.