Dispose Multiple Defects for a Serialized Product
Before you begin
- Ensure that you have configured the required disposition action reason tree in Plant Applications Administrator, and then linked the disposition action reason tree for selection in Non Conformance by using the appropriate script file.
- Add all the defects that you want to dispose to a plan.
About this task
Note: You cannot dispose multiple defects at the same time for a non-serialized product.
Procedure
- Search for the plan by performing one of the following steps:
- If the plan appears in the workspace or in the left pane, select the link.
- Enter the plan number in the Search box that appears in the left pane or in the workspace.
A list of defects added to the plan appear in the workspace. - Select
.
The Disposition window appears, displaying a list of serials/lots corresponding to the defects in the plan. The check boxes for all the serials/lots in the list are selected and disabled. - Provide values as specified in the following table.
Box Description Dispositions Select an option as described in the following table.
A value is required.Option Description CLEAR Select this option if the defects raised for the non-conformance are not considered as defects. (CTP) Continue to process Select this option if you want to allow work on the serials/lots, and then select the operation until which you can continue the work, in the USE UNTIL/REWORK OPERATION box. When you do so, the status of the operation during which the defect was raised changes from on hold to in progress, and the operation that you select in the USE UNTIL/REWORK OPERATION box changes to On Hold. Note: If the operation at which the non-conformance has been created on the serial/lot is the last operation in the route, you cannot select this disposition method.Note: When a non conformance is disposed as CTP to an operation in a mutually exclusive set, then all the operations in that mutually exclusive set will go on hold by default.SCRAP Select this option if you want to discard the defective serials/lots. USE AS IS Select this option to use the serials/lots in the operations as they are. SCRAP Select this option to discard the serials/lots. REWORK Select this option to rework on the serials/lots, and then select the operation during which the serials/lots should be reworked, in the USE UNTIL/REWORK OPERATION box. Note: In the list of operations to be reworked, the excluded operations from the mutually exclusive set will not appear.MRB Select this option to indicate that the defects must be reviewed by the material board, thus deferring the disposition to a later date. This will allow the quality team in your organization to determine the correct disposition method. USE UNTIL/REWORK OPERATION This box appears only for the following disposition methods: - ReworkNote: In the list of operations to be reworked, the excluded operations from the mutually exclusive set will not appear.
- Continue to processNote: When a non conformance is disposed as CTP to an operation in a mutually exclusive set, then all the operations in that mutually exclusive set will go on hold by default.
Select the operation until which the serial/lot can be processed. A value is required. After the serial/lot reaches the operation that you have specified, it must be disposed again.
DEFECT REASON Select a corrective disposition action reason and the associated subreasons, as applicable. Tip: In the Search box, enter a disposition action reason to search for, and then select the reason from the reasons list.ADDITIONAL INFORMATION Enter any relevant information, such as a URL, contact details of the supplier, or any information that is helpful to perform the root cause analysis of the non-conformance. - Rework
- Select Submit.
Results
Disposition Type | Result |
---|---|
Clear |
|
Continue to process (CTP) |
Note: When a non conformance is disposed as CTP to an operation in a
mutually exclusive set, then all the operations in that mutually
exclusive set will go on hold by default.
|
Use as is |
|
Scrap |
|
Rework |
Note: In the list of operations to be reworked, the excluded
operations from the mutually exclusive set will not
appear.
|
MRB |
|