ENTER BOM NAME/DESCRIPTION |
Enter the name or a description for the new BOM
formulation. |
BOM FAMILY |
Select a BOM family from the list to enable and populate
the Master BOM field. |
MASTER BOM |
Select the name of the master BOM to which the new BOM
formulation belongs. |
MATERIAL |
Select the materials for which the BOM formulation will
be created/available. You can select the Select All
check box if you want to include all. |
ENGINEERING UNITS |
Select appropriate engineering units (also known as Units
of Measure) for the material selected in the previous
field. |
QUANTITY PRECISION |
Enter the valid number of decimal places for the
value. Note: You can enter a precision up to 10 decimal
places. |
QUANTITY |
Enter the quantity for the BOM formulation. This must
follow the defined precision value. |
EFFECTIVE DATE |
Using the date picker, select the effective date and time
of the formulation. Note: You can use a BOM formulation only
from its effective date. |
EXPIRATION DATE |
Select the check box to enable the date picker. Using the
date picker, select the date and time at which the
formulation will expire. |