Show or Hide Tabs
You can configure to show or hide tabs for an application.
Procedure
- Log in to the Plant Applications Web Client.
-
Select
.
The Configuration page appears with Standard Tab selected by default. The Standard Tab page lists all the available default and custom tabs for a selected application. - In the Standard Tab page, from the Application section in the left pane, select an application for which you want to show or hide tabs.The list of default and custom tabs appears. The following table provides information on each column in the table.
Column Description ON/OFF You can switch the toggle to either show or hide the associated tab in the selected application. TAB NAME The name of the tab along with its description that appears in the selected application. For Custom tabs, appears as a suffix to the tab name. You can create custom tabs using the Custom Tab page.
REORDER Use or
to shift the tab names up or down to arrange them in a sequence depending on how you want them to appear in the selected application.
- Select Update to save your changes.You can navigate to the corresponding application to verify if the changes you made are reflected.