Access a Whisker Chart
Procedure
- Access the autolog history of the activity for which you want to access the Whisker chart.
-
Select
.
The Whisker chart appears, plotting the variable value, along with the following statistical items:Statistical Item Icon Represents the Lower Quartile point at left and the Upper Quartile point at right with median represented by a vertical line. Represents the Upper Reject limit beyond which the variable value is rejected. Represents the Lower Reject limit below which the variable value is rejected. Represents the Target value for the variable. Represents the Actual value you entered for the variable. Note: The lower, median, and upper quartile points are calculated based on the values entered for the variable in the last 20 completed activities associated with the same event. If no historical data exists for a variable, the values do not appear. The values for upper and lower reject limits are based on the Plant Applications Administrator settings.Tip: You can pause over an icon to view the value of the statistical item.
What to do next
- As needed, add a comment for the activity or a variable.
- Complete the activity.