About Operations
An operation consists of tasks that you perform while producing a product (for example, drilling, turning, and painting). When you define a route, you define a set of operations that must be performed to complete the route. Each operation is associated with one or more pieces of equipment that are defined in Plant Applications.
You can also specify whether the operation requires clocking on. For example, if clocking on and clocking off is already tracked in an ERP system, it is not required to clock on again using Plant Applications Web Client. In that case, when creating an operation for a route, you can specify that the operation does not clocking on.
Using Route Editor, in addition to creating an operation, you can copy, modify, and delete an operation.
Operations in a Motor Assembly Route
Suppose you want to create a route for assembling the parts of a motor. The following tasks are involved in completing the route:- Shell turning
- Stator and endshield assembling
- Rotor and endshield assembling
- Testing
- Painting
- Powder coating (a mutually exclusive operation for painting)
- Packaging
Operation | Equipment |
---|---|
Shell turning | The lathe machine |
Stator and endshield assembling | The pneumatic bolt tightener |
Rotor and endshield assembling | The pneumatic bolt tightener |
Testing |
|
Painting | The spray paint workstation Note: Both painting and powder coating are mutually exclusive
operations. |
Powder coating | The powder coating workstation Note: Both painting and powder
coating are mutually exclusive operations. |
Packaging |
|