Asset Reserved Attributes
About Reserved Attributes for an Asset Instance
GE Digital APM reserves certain attribute names in order to standardize similar functionality across all applications. As a result, specific default attribute names are reserved for system use.
Reserved attributes are predefined properties commonly used for node asset instances when they are ingested. Reserved attributes for an asset instance are inherited from the associated asset classification. You can add or edit values for the predefined attributes in an asset instance.
Values can be single or multiple. Multiple values are only available for the reserved attributes that show the List values link. List values options are created during asset configuration and cannot be added by you. The value format must match the data type configured for the asset instance. The data type for a reserved attribute cannot be changed by you.
Values for reserved attributes may be left blank.
For more information on the different scenarios, refer to the Expected Behavior for Reserved Attributes documentation.
Sort Reserved Attributes for an Asset Instance
You can sort reserved attributes for an asset instance by the attribute name.
About This Task
Procedure
- In the module navigation menu, go to Assets > Asset Instances.
- Select an asset context using the context browser.
- In the Reserved Attributes section, select Attribute Name.
Results
Export Reserved Attributes for an Asset Instance
Procedure
- In the module navigation menu, go to Assets > Asset Instances.
- Select an asset context using the context browser.
- In the Attributes section, select Export All Attributes.
Results
Add or Modify Reserved Attribute Values for an Asset Instance
You can enter or modify reserved attribute values for an asset instance.
About This Task
You can enter a new value or modify an existing value for a reserved attribute. Some reserved attributes may have multiple values, in which case the attribute includes displaying a drop-down list in place of a single value. You can select the icon to display the list of values as a table. You can select
to modify the displayed values.
Reserved attributes have predefined formatting which cannot be modified. You cannot add or delete a reserved attribute.
Field Name | Display Name | Type | Default Value |
---|---|---|---|
state | State | KeyValue |
|
status | Status | KeyValue |
|
Procedure
- To enter or modify a single value for a reserved attribute:
- To enter or modify multiple values for a reserved attribute:
Remove Values from Reserved Attributes for an Asset Instance
You can remove values from a reserved attribute for an asset instance.
About This Task
You can remove an existing value for a reserved attribute. You can remove multiple existing values for a reserved attribute that contains . Reserved attributes have predefined formatting which cannot be modified. You cannot add or delete a reserved attribute.
Procedure
- To remove an existing value for a reserved attribute:
- To remove multiple existing values for a reserved attribute: