Asset Custom Attributes
About Custom Attributes for an Asset Instance
You can define custom attributes for an asset instance.
When you ingest an asset, you can define custom attributes for an asset instance. Each attribute uses a format and a value that helps define how the asset behaves.
For example, suppose you have a reserved attribute that designates the model of a physical piece of equipment, and you want to include the model number as an attribute. You can use Custom Attributes to add a model number as an attribute for the selected asset instance.
Sort Custom Attributes for an Asset Instance
You can sort custom attributes for an asset instance by the attribute name.
About This Task
Procedure
- In the module navigation menu, go to Assets > Asset Instances.
- Select an asset context using the context browser.
- In the Custom Attributes section, select Attribute Name.
Results
Export Custom Attributes for an Asset Instance
Procedure
- In the module navigation menu, go to Assets > Asset Instances.
- Select an asset context using the context browser.
- In the Attributes section, select Export All Attributes.
Results
Filter Custom Attributes for an Asset Instance
You can filter custom attributes for an asset instance based on attribute names.
Procedure
Add a Custom Attribute for an Asset Instance
You can add a custom attribute to a selected asset instance.
About This Task
Creating a new custom attribute allows you to define properties for the selected asset. Attributes may include a unit of measure next to the entered value on the asset instance view. Some attributes may include multiple values in a list of values. All custom attributes are modified on the asset instance view.
Procedure
Modify a Custom Attribute for an Asset Instance
You can modify a custom attribute for a selected asset instance.
About This Task
Use this procedure to modify the data type and value of custom defined attributes for an asset instance.
You can modify a custom attribute by reentering a Value in the table, or by selecting and modifying the format and value from there.
Procedure
- To modify a value in custom attributes for an asset instance:
- To enter or modify multiple values for a custom attribute:
Delete a Custom Attribute from an Asset Instance
You can delete a custom attribute for a selected asset instance. However, if an attribute is defined in the classification, and have been inherited to an asset instance, you cannot delete the attribute from an asset instance.
About This Task
Use this procedure to delete a custom attribute from an asset instance.