Performing Offline License Removal
When the Local License Server is not connected to the Cloud License Server, you can use a connected computer to process the information required to remove licenses from the offline Local License Server.
Before you begin
- Before you remove any licenses, save their activation codes in case you want to reactivate them in the future.
- Review the offline license management process instructions in the Complete Offline Process page.
- Verify you have access to a computer connected to the Cloud License Server and that computer has the Local License Server Administration Tool installed.
About this task
- From the offline Local License Server, create a request file with the license codes for the Cloud License Server to remove. This generated request file in the permanently offline computer is transferred to a computer connected to the internet.
- From the online computer, request a response file, which sends the request file to the Cloud License Server for verification. The Cloud License Server returns a response file containing the needed information to remove the licenses on the Local License Server. The response file generated in the computer connected to the internet is transferred to the computer permanently offline where the request file was originally generated.
- Within 24 hours of receiving a response file, transfer the file into the offline Local License Server to remove the licenses.
Procedure
-
To create a request file in the offline Local License Server, do the
following:
-
From the online computer, send the request file for a verification response by
selecting 2, Generate a response file from an online
computer on the Complete Offline
Activation tab and do the following:
-
From the offline Local License Server, remove the licenses by selecting 3,
Use the response file to update licenses on the original offline
server on the Complete Offline Process
tab and do the following:
- Navigate to the response file.
- Select Update Licenses.
- To verify the licenses were removed, select the Licenses tab and then Update Table.