Command-Line Operations
You can use the Server Console commands to activate and remove multiple license codes on the Local License Server.
To execute the Server Console, use the following syntax:
ProficyServerConsole.exe [-INIFILE=[PATH]file.ini] [-TIMEOUT=timeout]
Note:
Providing specifications inside [] is optional.
To view the Server Console command-line examples, enter the following command:
ProficyServerConsole.exe -Help
If an error occurs when running a command, an error code and message displays on the Server Console. For more details on an error, see the Server Console log file.