Server Console Parameters

Use the Server Console parameters to specify timeout values and the location of the INI file.

The optional -TIMEOUT parameter uses the specified communications timeout period when connecting to the local license server and the GEIP Web Server. If your server communication is timing out or if you have a big list of codes to add to the local license server, you can use this command line option to increase the timeout period.

You can modify the -TIMEOUT parameter using the following syntax:

-TIMEOUT=timeout
Note:
The default timeout period is 30 seconds. You must specify a timeout value between 30 and 250 seconds. You can start with 60 seconds and increase the value by 30-second intervals, if needed.

The optional -INIFILE parameter specifies the filename and path of the INI file you are using to manage licenses.

You can modify the -INIFILE parameter using the following syntax:

-INIFILE=[PATH]file.ini
Note:
If you do not use -INIFILE, the tool looks for the filename “ProficyServerConsole.ini” in the current folder, and then in the My Documents folder.

If you do not specify the [PATH] of the INI file, the tool looks in the current folder, and then in the My Documents folder.