Lookup Object

The Lookup object is an animation object that uses the input value to perform either a range comparison or exact match to a table and provides the output value based on the values in the table. It contains information about the connection between the data source and the input property of the lookup object, and the output property of the lookup object and the animated property of the object being animated. For example, you can use the Lookup object to blink on a new alarm.

 

Methods

Properties

Events