SetSource Method

Sets up the source connection properties for the animation object. This method is used instead of directly setting the animation object's source property if additional properties have to be specified for the connection.

Syntax

object.SetSource bstrExpression, [bUseAnyway], [vaUpdateRate], [vaDeadband], [vaTolerance], [vaConnectionFlags]

Properties

The SetSource method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

bstrExpression

String. The expression representing the source.

bUseAnyway

Boolean. (Optional) Specifies whether to use a connection if the source doesn't exist. Default = False.

aUpdateRate

Float. (Optional) The value at which to set the update rate for the connection.

aDeadband

Float. (Optional) The value at which to set the deadband for the connection.

aTolerance

Float. (Optional) The value at which to set the tolerance for the connection.

aConnectionFlags

Long. (Optional) Reserved Word.

Remarks

The vaTolerance parameter only applies in expressions and exact match tables.

 

Example

Applies To