The Linear object is an animation object that converts data from one form into another, effectively performing standard signal conditioning. It contains information about the connection between the data source and the input property of the linear object, and the output property of the linear object and the property of the object being animated. For example, you can use the Linear object to animate the tank level of a picture of a tank by mapping it's high and low EGU to reflect the scale of the picture.
Methods
DoesPropertyHaveTargets Method
GetConnectionInformation Method
GetConnectionParameters Method