FixedTime Property

Specifies a fixed time in the Chart,PenGeneralDataSet Object, or Formatted Object ,Line,Lookup Object,.

Syntax

object.FixedTime [= DateTime]

Example

#1/1/2000 12:00:00 AM#

Properties

The FixedTime property syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

DateTime

The fixed time.

Remarks

FixedTime is a one-shot property.

The default value for the FixedTime property is the time at which thePen or Chart was created. Although this property is passed as a complete Date and Time datatype, the Date portion is ignored.

This property is not impacted by any Global Time Control property settings.

 

Applies To