Modify Method

Displays the Modify Block dialog box for the specified block.

Syntax

object.Modify bstrFullyQualifiedName, bReadOnly, iStatus

Properties

The Modify method syntax has these parts:

Part

Description

object

An object expression that evaluates to an object in the Applies To list.

bstrFullyQualifiedName

String. The fully qualified name of the block you want to modify.

bReadOnly

Boolean. True if the block can only be showed, False if the block can be modified.

Istatus

Long. Returns the error status value.
Return values are:
0 – OK
1 – Syntax error
2 – Data Undefined
3 – Data type mismatch

 

Example

Applies To