Adds a new level to the table (Lookup object).
Syntax
object.AddLevel pInput1, pOutput1, [pInput2], [pOutput2]
Properties
The AddLevel method syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
pInput1 |
Variant. The first input parameter. Used as the lookup value when performing exact match lookups, and the minimum value for range comparison lookups. |
pOutput1 |
Variant. The primary output value. |
pInput2 |
Variant. (Optional) The second input parameter. Used as maximum value for a range lookup comparison. |
pOutput2 |
Variant. (Optional) The secondary output value for this level. This value is used by the lookup object as the “blink to” value at this level. |