Specifies the tolerance for exact match Lookup tables.
Syntax
object.Tolerance [= Single]
Properties
The Tolerance property syntax has these parts:
Part |
Description |
object |
An object expression that evaluates to an object in the Applies To list. |
Single |
The tolerance value. |
Remarks
The tolerance will work just like in an expression. If the value is within +/- tolerance, the value will pass the condition imposed – in this case equality.
For example, the user sets up an exact match table such that an object is green when the value is 0 and red when the value is 1. Most likely the value will end up being 0.0000009, and therefore the object may never be green. Tolerance will prevent this.