Testing Connections
Test Connection function is provided on the OPC UA server connection's Details panel. The test connection function is initiated from the toolbar button .
The test makes an attempt to reach to the end point URL provided in the Connection Details panel and on successful connection comes back with the test status and populates into the end point URL field with a check mark; on failure to connect the same field is highlighted in red with failure a reason.
The following figure displays a successful test.