PRT_STATUS
The PRT Status ( prt_status ) configuration file is used to assign a status code for each valid region status; for example, capacity, sequential error, invalid or unknown type, etc. Similarly, a record is configured for each valid item status; for example, hold, no-hold, delayed, etc. A number of statuses have predefined records, and you may configure additional records to define other status types.
OPTIONAL FILE
The fields are:
No. | Field Name | Description | Data Type | Entry Example |
0 | status_code | Unique code to identify the status of the region or item. | 8 characters | CTRLWTRK |
1 | code_type | Unique code representing what you are defining a status code for, as follows: 0 = Region Status Code 1 = Item Status Code 2 = Reserved | One byte | 0 |
2 | code_desc | Textual description of the status code. | 40 characters | Blank |
3 | code_label | Text to display with the status code for user recognition. Must be unique. | 16 characters | Control w/track |
4 | bit_set | Bit to be set by PRT that will represent this status code. | Long word | 22 |