PRT_DISP_PT
The PRT Display Point ( prt_disp_pt ) configuration file is used to define the Item Type quantity in a region to be displayed through a setpoint. This file must be configured when prt_grd is configured.
OPTIONAL FILE
The fields are:
No. | Field Name | Description | Data Type | Entry Example |
0 | region_id | Unique name for the tracking region. | 16 characters | RINSE1_NOR |
1 | item_type_id | Unique name for the item type. | 16 characters | WSH_FRAME |
2 | qty_ptid | Unique name for the setpoint to display the item type quantity in the region. | 55 characters | R1_CTQ |