PRT_SERVICE
The PRT Service ( prt_service ) configuration file is used to identify each Production Tracking Service.
REQUIRED FILE
The fields are:
No. | Field Name | Description | Data Type | Entry Example |
0 |
prt_svc_id
|
Specifies the PRT Data Collector Resident Process Service ID. This must be identical to the ID in service.dat . | 32 characters | APRT_DC |
1 |
prt_search_order
|
Indicates the order in which this service will be searched for information static to other configured PRT Services. | 1 byte | 1 |
2 |
ext_item_svc_id
|
Service ID of the external process providing item tracking data. | 32 characters | Blank |
3 |
ext_hold_svc_id
|
Service ID of the external process providing hold information | 32 characters | Blank |
4 |
det_reg_alrmid
|
Alarm ID for items placed in detainment region. | 32 characters | PRT_DET_REF_FULL |
5 |
region_lock_alrmid
|
Alarm ID generated when an item enters IN-LOCKED region, or exit OUT-LOCKED region via a point-based move. | 32 characters | PRT_ITM_THRU_LCK |
6 |
region_cap_alrmid
|
Alarm ID when the maximum number of item carriers in the region are exceeded. | 32 characters | PRT_REG_CAP |
7 |
loc_cap_alrmid
|
Alarm ID when the maximum number of items at a single region location / item carrier have been exceeded. | 32 characters | PRT_REF_LOC_CAP |
8 |
seq_err_alrmid
|
Alarm ID when an item is out of sequence at a region exit transition indicator. | 32 characters | PRT_REG_OOS |
9 |
item_hold_alrmid
|
Alarm ID when an item arrives in a tracking region and is determined to have an item-hold specification. | 32 characters | PRT_ITM_WITH_HLD |
10 |
invalid_type_
alrmid
|
Alarm ID when an invalid item type is detected. | 32 characters | PRT_INVALID_TYPE |
11 |
unknown_type_
alrmid
|
Alarm ID when an unknown item type is detected. | 32 characters | PRT_UNKNOWN_TYPE |
12 |
invalid_id_alrmid
|
Alarm ID when a serialized item enters a region and information cannot be retrieved for that item. | 32 characters | PRT_INVALID_ITEM |
13 |
region_not_empty_
alrmid
|
Alarm ID when all items have not left a disperse tracking region and new items have arrived in the region. | 32 characters | PRT_DSP_NOT_MPTY |
14 |
Batch_queue
|
NOT USED | Not used | Blank |