Rounds Pro

Deploy Rounds Pro for the First Time

The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

StepTaskNotes
1

Review the data model to determine which relationship definitions you will need to modify to include your custom Equipment and Functional Location families. Modify any relationship definitions as needed via Configuration Manager.

This step is required only if you have asset data in families outside of the baseline Equipment and Functional Location families.
2

Assign Security Users to the following Rounds Pro Security Groups:

  • MI Rounds-Pro Administrator 
  • MI Rounds-Pro Mobile User
This step is required.
3Install the Rounds Pro mobile app on the mobile device that you plan to use for data collection.This step is required only if you will use a mobile device for data collection. For information on installation of Rounds Pro on mobile devices see the following sections:
4Set the local time zone on the mobile device that you will use for data collection, typically the user time zone.This step is required only if you will use a mobile device for data collection.

Upgrade or Update Rounds Pro to V4.6.10.0.0

About This Task

The following tables outline the steps that you must complete to upgrade this module to V4.6.10.0.0. These instructions assume that you have completed the steps for upgrading the basic APM system architecture.

These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.

Procedure

Upgrade from any version V4.6.0.0.0 through V4.6.9.0.0

This module will be updated to V4.6.10.0.0 automatically when you update the components in the basic APM system architecture. No additional steps are required.