GE: World Leader in Naval Electric Drive Power and Propulsion

BUSAN, REPUBLIC OF KOREA - October 21, 2019 – GE’s gas turbine and electric drive power and propulsion systems are proven to meet the most demanding needs of world navies. Today at the MADEX International Marine Industrial Defense Exhibition, GE is highlighting its power and propulsion capabilities as they apply to two new proposed Republic of Korea (ROK) Navy programs: the KDDX destroyer and the LPX-II amphibious assault ship.

“GE is the only company that offers a full spectrum of gas turbine and electric drive propulsion solutions including mechanical drive, hybrid electric drive (HED) or integrated full electric propulsion (IFEP). Together, GE Aviation-Marine and GE Power Conversion are world leaders, having provided naval power and propulsion systems for 37 navies onboard 715 ships,” says Kris Shepherd, Vice President, General Manager, GE Aviation–Marine, Evendale, Ohio. “To date, GE has supplied the ROK Navy with 186 marine gas turbines for 107 ships. Our longstanding in-country partner Hanwha Aerospace co-manufactures the engine components for the ROK’s naval and industrial gas turbines,” Shepherd added.

For the 8,000-ton ROK Navy’s KDDX destroyer, GE offers proven solutions for the two considered propulsion configurations: HED or IFEP. The HED system would use the 3.4 MW shock tested motor designed for the United Kingdom Royal Navy’s Type 26 frigate. The IFEP system would be nearly identical to the electrical system GE designed for the U.K.’s Type 45 destroyer. Both propulsion systems would use dual GE gas turbines to meet survivability and efficiency needs.

“Whether HED or IFEP is selected, GE is proposing proven equipment. Our HED motor is the right size motor for KDDX and GE is the only manufacturer to build a naval motor over 2.5 MW. “

“The IFEP is an attractive solution to satisfy the larger and ever-increasing power demands of weapons and radar systems and when operational flexibility and efficiency are important factors. GE’s IFEP solution uses fourth generation advanced induction motors, shock-proof drives and our generator - coupled to a reliable GE LM2500 gas turbine - to provide a low-risk, fully compliant solution,” says Andy Cooper, U.K. Managing Director of GE Power Conversion. “The KDDX IFEP solution with our electrical system integration expertise is a natural first step as the ROK Navy progresses to a scaled-up IFEP system on the larger LPX II ship,” Cooper stated.

GE’s highlights during MADEX include these power and propulsion capabilities and recent product enhancements that benefit the ROK Navy KDDX and LPX-II ship programs:

  • GE is the world leader in IFEP solutions and can leverage past programs including the U.K. Royal Navy Type 45 destroyers and Queen Elizabeth class aircraft carriers, and the United States Navy’s DDG 1000 destroyer
  • GE’s IFEP solution for the ROK Navy offers a ship with superior operational flexibility and fuel economy, power for future growth and optimal survivability/redundancy by using two right-sized gas turbines.
  • For nearly 30 years, GE has supported the U.K. Royal Navy with HED technology; collaborations include the pioneering Type 23 class in the 1990s and now the HED system for the Type 26 Global Combat Ship.
  • Complementing its engineering capability is GE’s Marine Power Test Facility which is the only commercial land-based facility in the world capable of full-scale testing of integrated navy systems and ship architectures.
  • GE’s power dense marine gas turbines offer best in-class reliability with low lifecycle costs. GE’s lightweight composite module recently received full qualification from the U.S. Navy after completion of a series of tests including barge shock testing. Compared to its steel predecessor, the new gas turbine module offers a weight reduction of over 2,000 kg, elimination of corrosion, is 60% quieter, and has wall temperatures that are 25°F to 50°F degrees cooler.

 

About GE

GE (NYSE: GE) drives the world forward by tackling its biggest challenges: energy, health, transportation—the essentials of modern life. By combining world-class engineering with software and analytics, GE helps the world work more efficiently, reliably, and safely. For more than 125 years, GE has invented the future of industry, and today it leads new paradigms in additive manufacturing, materials science, and data analytics. GE people are global, diverse and dedicated, operating with the highest integrity and passion to fulfill GE’s mission and deliver for our customers. www.gevernova.com

About GE Power

GE Power is a world energy leader providing equipment, solutions and services across the energy value chain from generation to consumption. Operating in more than 180 countries, our technology produces a third of the world’s electricity, equips 90 percent of power transmission utilities worldwide, and our software manages more than forty percent of the world’s energy. Through relentless innovation and continuous partnership with our customers, we are developing the energy technologies of the future and improving the power networks we depend on today. For more information please visit www.gevernova.com/power, and follow GE Power on Twitter  and on LinkedIn.

 

For general press enquiries, please contact us here