Uninstall the reporting database

When you uninstall reporting, the database remains intact; however, you lose the ability to synchronize the data from your production database. Uninstalling reporting does not affect the production database or the data contained in it; you can still run reports on the data stored in the database.

Procedure

  1. From the Control Panel, click Programs and Features.
    The Uninstall or change a program dialog box appears, displaying all of the programs installed on the computer.
  2. Select Reporting, and then click Uninstall.
  3. In the confirmation message box, click Yes.
    The Uninstall Reporting message box appears stating, "Uninstalling the Proficy Reporting application will not remove the Reporting database or the SQL Agent job from SQL Server. For a complete uninstall of this application, these should be removed manually following the uninstall."
  4. Click OK.