Configure Component Services
If your production database is on a different computer than the Reporting Database, the following configuration changes are required.
Before you begin
Important:
You can perform these steps either before or after installing the Reporting Database; however, you must complete these configuration changes before you run your reporting data synchronization.
Note:
For this procedure, your production database server is the "server," while the reporting database server is the "client."
Procedure
- Verify that the Distributed Transaction Coordinator service is running on both the server and client computers.
- From the Start menu, point to Administrative Tools, and then click Services.
- If the Distributed Transaction Coordinator service is not running, right-click it, and then click Start.
- On the server computer, from the Start menu, point to Administrative Tools, and then click Component Services.
- In the left navigation tree, click Component Services, and then expand Computers.
- Right-click My Computer and select Properties.The My Computer Properties dialog box appears.
- Click the MS DTC tab.Important:If you are using Windows 7, Windows Server 2008, or Windows Server 2012, you must use the following path to retrieve these computer properties: Component Services> Computers>My Computer>Distributed Transaction Coordinator>Local DTC.
- Click Security Configuration.The Security page appears.
- Select the following check boxes:
- Network DTC Access
- Allow Remote Clients
- Allow Inbound/Outbound Administration
- Enable Transaction Internet Protocol (TIP) Transactions
- Click OK.A message appears, stating that "MS DTC Service will be stopped and restarted. All dependent services will be stopped. Please press Yes to proceed." Click Yes.
- In the My Computer Properties dialog box, click OK.
- If required, reboot your production database server.Note:We recommend that you reboot your production database server.
- On the client computer, repeat steps 2-6.
- Select the Network DTC Access and Allow Inbound/Outbound Administration check boxes.The DTC Service is stopped and restarted.
- Restart the client computer.
- Verify that the Distributed Transaction Coordinator service is running on both the server and client computers, and, if required, repeat step 1.