Sign task actions electronically
You may be required to add an electronic signature to a task or task step action, such as priority, cancel, jump, and reassign, in order to authorize particular activities in the Task List.
About this task
Note:
If a Windows user is required to electronically sign a form or a task list action, the user logged into the Workflow client must also be a Windows user. A Windows user cannot sign forms when a Workflow user is signed in to the client.
Procedure
- In the Task List, navigate to a task or task step action.
- In the control bar, click the Actions button.
- Click the button for the action that you want to perform, and then enter content for the action.
- Click Sign.
- In the Performer Signature area, enter the required information to authorize the action.
For example, if the workflow author configured the Form activity to use the Operator group as valid performers, then only a user who is a member of that group can sign as a performer.
- Proceed based on performer signature verification requirements.
If the performer signature... Then do this... requires verification Click Sign to display the Verifier Signature area, and then go to step 5. If you do not want to continue, click Cancel. does not require verification Click Sign and Submit. Note:In this scenario, this action represents the last step of the electronic signature process, and you do not have to complete the remaining steps of this procedure. - In the Verifier Signature area, enter the required information.For example, if the workflow author configured the Form activity to use the Supervisor group as valid verifiers, then only a user who is a member of that group can sign as a verifier. The verifier signature cannot be completed by the personnel resource associated with the same user account as the one for the performer signature.
- Collect the verifier's electronic signature.
For a... Click... task/task step action Sign and OK form Sign and Submit - Optional: To make changes before submission, click Cancel Signing to close the electronic signature panel. When the changes are complete, you must restart the signing process.