Override a Computer's Startup Options

You can override the configurations for a specific computer with specialized settings for individual users who log into this computer, or for computers with specialized settings for individual users who log into any computer configured to use global default settings.

Procedure

  1. In the navigator, click Proficy System > Proficy System > Computers.
  2. From the Computers list, select the computer that you want to configure.
    Tip: If you are configuring settings for all computers in your system or a subset of those computers, you can skip this step. However, you can still configure global default settings if you select an individual computer.
  3. In the Displays panel, select the editor you want to use.
    To configure user overrides for...Select
    an individual computerComputer Editor
    all computers or a subset of computers in your systemDefault Computer Editor
  4. Click the User Overrides tab.
  5. In the User Overrides list, add a user you want to create overrides for.
  6. Optional: Select or clear the Show Solution Panel check box and/or the Show Navigator check box.
    Note: If you clear these check boxes, you must define a startup solution and display.
  7. Optional: To change the startup object:
    1. Select the Navigate Users on Login check box.
    2. Click Change Startup Object, and then select the object to use as the startup object.
    The name and path of the startup object appear.
  8. Optional: To change the startup solution and display:
    1. Select the Users will be started in a specific solution/display check box.
    2. Click Change Startup Solution, and then select the solution and display to use when the Workflow starts up.
      The names of the startup solution and display appear.
  9. Click Save.