Custom User Solutions and Displays

Workflow provides the ability to create custom user solutions. User solutions allow you to organize the displays that you create.

User solutions are displayed in the solution panel as separate and distinct solutions. When you create a user solution, it automatically appears in the solution panel.

You can configure a user display to be:

  • Available only in the navigator.
  • Visible in the navigator and in the Displays panel under a user solution.
  • Context aware, and if so, which resource and user solution it works with.
Note:
When a context aware resource is selected in the navigator, its compatible views are highlighted in the Displays panel. You can then select a compatible view or display to begin working with the resource. For more information, see Display Panel.

When a user solution is created, the Display Editor appears with a series of icons that can be selected to organize user displays. The selected icon appears beside the user solution name in the solution panel.