Custom (User-Created) Solutions

The Display/View Config tab is used to configure user-created solutions to be available in the Displays panel and to associate user displays with those user solutions.

The following table describes the available attributes.

AttributesValueDescription
Display ConfigurationUser-definedSelect an option to indicate whether the selected user display is available in the solution panel.

If you select This display is available in the solution panel, you must select a user solution from the list to associate the user display with.

Context View Configuration check boxUser-definedSelect this check box to indicate that the current user display will be context aware. That is, when the user display is selected in the navigator, the compatible views are highlighted in the solution panel.

This check box is available only when you select the Display Configuration option, The Display is available in the solution panel.

If you clear this check box, the user display is still associated with the selected user solution; however, it is not context aware. That is, the display is not highlighted in the solution panel, nor does it appear in the Show Compatible list.

Note:
A user display can be associated with only one user solution, but can be associated with multiple object types.
Object TypesUser-definedLists the object types you can associate with the current user display. If the user display is already associated with an object type, that object type is not available to select from the list for this user display.

Object types are available for selection only when the Context View Configuration check box is selected.

Included Object TypesUser-definedLists the object types that the current user display is associated with.
Excluded Object TypesUser-definedLists the object types that the current user display cannot be associated with.