Override Startup Options
The User Overrides tab allows you to override the startup options for specific users who log on to the selected computer or for specific users who log on to any computer that is included in a global default configuration.
Overrides that are configured using the Computer Editor are specific to the selected computer. Overrides that are configured using the Default Computer Editor are global; that is, the specified user can log on to any computer that is included in a global default configuration and the startup options defined for that user will be displayed.
The following tables describe the information available on the UserOverrides tab, where you can configure a custom client layout for individual users.
Attribute | Value | Description |
---|---|---|
List | User-defined | Displays a list of users that have user overrides configured on the selected computer. |
Add User | N/A | Click to add a user that you can configure user overrides for on the selected computer. |
Delete User | N/A | Click to delete a user from the overrides list. Note: When a user is removed from the User Overrides list, the default layout configured for the selected computer will be displayed the next time this user logs on to that computer. |
Layout Configuration
These options specify the client panels that will be visible on this computer when the selected user logs on.
Options | Description | |
---|---|---|
Show Solution Panel |
Select this check box to show the Solution Panel when the selected user logs in on this computer. If you clear this check box, the Solution Panel is hidden for the selected user at log in on this computer, and you must select a startup solution and display for the user. | |
Show Navigator |
Select this check box to show the navigator when the selected user logs in on this computer. If you clear this check box, the navigator is hidden for the selected user at log in on this computer, and you must select a startup object for the user. |
Startup Object
These options specify the object that this computer will start at when the selected user logs on.
Options | Description | |
---|---|---|
Navigate Users on Login |
Select this check box to start the user at a specific object on this computer.
Note: You must select this check box and define a startup object if the Show Solution Panel check box is cleared. | |
Change Startup Object |
Click to open the Universal Browser to select the startup object to display at log in for this user on this computer.
Note: You must select a startup object if the Show Solution Panel check box is cleared. |
Startup Display/Solution
These options specify the display and solution that will be displayed on this computer when the selected user logs on.
Options | Description | |
---|---|---|
Users will be started in a solution/display |
Select this check box to start the user with a specific display and solution on this computer.
Note: You must select this check box and a startup display/solution if the Show navigator check box is cleared. | |
Change Startup Solution |
Click to open the Universal Browser, where you can select the startup display/solution to display at login for this user on this computer.
Note: You must select a startup display/solution if the Show Navigator check box is cleared. |