Create a fault resource

Configuring a fault allows you to assign a message to a user-defined fault in order to provide more information about the issue.

Before you begin

Note:
A resource must already have been added in order to select it from this list. For more information, see Add a resource to the workflow model.

Procedure

  1. In the navigator, click Workflow.
  2. In the Folders list, select a resource type, such as Workflows, Subprocesses, Schedules, User Activities, Categories, Completion Codes, Faults, or Filters.
  3. In the resource type list, select a resource.
  4. In the Displays panel, click Workflow Management > Workflow Editor.
  5. In the Fault Message field, enter the message you want displayed when the fault occurs.
  6. Click Save.